(0)| 8/30/2018 2:28 PM | |
|
Posts: 20 Rating:
|
Hello, I have migrated a project of panel TP170B from ProTool to WinCC flex 2008 sp2 and then to WinCC Advanced v14. Then I have download the migrated project to KTP700 Comfort. Everything works like on the old panel, I can see same process values, alarms and events. The machine works normally. The only problem is that I get SF LED on and BF1 LED blinking on my CPU 317. If I disconnect KTP700 Comfort and reconnect TP170B, I get only the RUN LED and DC5V on like it should be. In the TIA WinCC advanced v14, I have same settings for Profibus (Profile is User-Defined) like in the old project. I have also select the right Profibus address for the new panel. In the attached file you can find what was in the diagnostic buffer of CPU. Can you help me please. Thanks BR Tomaž AttachmentDiagnose.txt (389 Downloads) |
Follow us on