9/12/2018 10:50 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, From the attached drawing & motor details, the DC motor is series wound type DC motor i.e. its armature & field windings are connected in series as such user cannot directly configured the standard DCM, it needs to select 6RA80..-..S22 type DCM. Please refer Operating series-wound or compound-wound motor FAQ for better understanding. |
Last edited by: Jen_Moderator at: 9/12/2018 1:21:38 PMOptimized link. |
|
This contribution was helpful to
1 thankful Users |
9/12/2018 11:28 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 112 Rating:
|
Hi, Is there any possibility that a normal DCM can be converted to a S22 type DCM .
|
Thanks |
|
Follow us on