(0)| 9/9/2008 3:42 PM | |
|
Joined: 4/6/2006 Last visit: 11/21/2025 Posts: 604 Rating:
|
Hi Henk, No it's only supporting ISOonTCP. For an ISO Connection you will need to use a CP443-1. Check the list in the following FAQ to see which one is interesting. What differences exist in the SIMATIC S7-400 series Ethernet CPs? And here is a clear FAQ which describes the possibilities with the onboard ethernet port. What are the commonalities and differences between configured communication connections and the open Ethernet communication? |
|
Best regards, |
|
| 9/10/2008 11:39 AM | |
|
Posts: 2 Rating:
|
Thanks for the quick reply! |
Follow us on