(0)| 9/25/2018 1:37 PM | |
|
Joined: 10/11/2006 Last visit: 1/20/2026 Posts: 6071 Rating:
|
Dear Hence, when triggering the test stop, the motor switches into a no-torque condition as described in the FHS G120 (https://support.industry.siemens.com/cs/document/109757227), page 180. We do not recommend doing this when the drive is turning, on the next page is clearly stated that the motor needs to be at standstill. The automatic test stop is only possible with S120, see FHS S120 (https://support.industry.siemens.com/cs/document/109760403), page 86. For the G120 you have to actively start the test stop, e.g. every shift, once a day, once a week … This can be done via PLC or digital input on the drive. This is also applicable to the feedback when the next test stop should be performed. |
|
With best regards, |
|
Follow us on