(0)| 9/25/2018 3:08 PM | |
|
Posts: 1 Rating:
|
Hi I am going to use TM41 as well, but I am not replacing the module, I am adding it as new using Starter, I did in "topology", but I can not configure the parameters, the "wizard" option it is not displaying. I was reading and I found that I need to use scout software to program the TM41 but all the program is in "starter"... is it a way to set the parameters using starter or I need to use scout? Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/26/2018 3:38:04 PMNew subject after splitting |
|
Follow us on