(0)| 10/4/2018 8:27 PM | |
|
Joined: 2/5/2015 Last visit: 4/8/2025 Posts: 130 Rating:
|
Friends, I'm having a similar problem. I created some alarms, ERRORS and WARNINGS. Also, I created an alarmview, configuring to ALARM LOG (alarm_log_1 tag) displaying ERRORS and WARNINGS. (attached). When an ERROR occurs it pops up the PENDING ALARM windows and it works correctly. I press the acknowledge button and clean the error from the screen. Works ok! BUT when an WARNING occurs it doesn't pop up the pendind alarm window. I've tried the "rebuild all" suggestion but it didn't work, and actually it changed the size of the letters on the screen. So I returned my backup project. Does anyone have some suggestions please!? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/5/2018 1:30:33 PMNew subject after splitting |
|
Follow us on