(1)| 7/16/2018 8:19 AM | |
|
Joined: 6/17/2014 Last visit: 9/7/2024 Posts: 11 Rating:
|
Good morning, I have issue with password locked MP 177 6" Touch HMI afetr entering wrong password many times. I can backup and restore via prosave. and I have backup file. Afetr backup and restore also password is locked. The project file I have and open with wincc 2008 SP3 shows the bellow bessage. " the project was created with an incompatible or beta versin of WinCC flexible, it was last opened with V 1.4.0.0 (1.16.16) Open the project with a valid WinCC felxible version" Continue the version change and transfered project and OS update , Afetr transfer HMI shows connecting.... But not get connect. How can I reset the password and solve the problem. Please help. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/16/2018 1:15:37 PMNew subject after splitting |
|
Follow us on