9/26/2018 6:51 AM | |
Joined: 5/29/2018 Last visit: 1/28/2021 Posts: 11 Rating:
|
It worked great in the simulation! Tomorrow i'll install it in real. many thanks! grtz |
9/26/2018 6:53 AM | |
Joined: 5/29/2018 Last visit: 1/28/2021 Posts: 11 Rating:
|
If I need this again, how do I know what type of Logo! I have and what to do in soft comfort to get things work? |
10/24/2018 8:55 AM | |
Joined: 5/29/2018 Last visit: 1/28/2021 Posts: 11 Rating:
|
Hi there, it's been a time but due to overload of work I wasn't able to try the program out earlier. I still have the same problem as before. The logo! doen't react on the pressure transmitter. The value on the screen stays at 0.004 and 0.008 despite moving the transmitter up and down in the water. The incoming voltage varies from 0 V until 4,5 V if 1.8 m deep in tank. So that's normal since the transmiiter scales from 0 to 4 m. For one reason or the other the signal is not recognized by the Logo! ? I connected the 2 signal+ wires to I1 and I2. Any clue anyone? AttachmentPump_FS04.zip (375 Downloads) |
10/28/2018 6:43 PM | |
Joined: 5/29/2018 Last visit: 1/28/2021 Posts: 11 Rating:
|
Thanks, it says if 2 Ai's are enabled to put them on I7 ad I8. didn't know that. I'll try. |
Follow us on