(0)| 9/26/2008 8:49 PM | |
|
Posts: 1742 Rating:
|
Hello, You could use the so called "ascii driver".
criteria for data receipt. The end criterion defines when a complete message frame is received. The possible end criteria are as follows: ● Expiration of the character delay time The message frame has neither a fixed length nor a defined end-of-text character; the end of a message frame is defined by a pause on the line (expiration of character delay time). ● Receipt of the end-of-text character(s) The end of the message frame is marked by one or two defined end-of-text characters. ● Receipt of fixed number of characters The length of the receive message frames is always identical. |
Follow us on