(0)| 1/30/2019 1:40 PM | |
|
Joined: 8/25/2014 Last visit: 10/7/2025 Posts: 172 Rating:
|
Dear #DP, As you mentiond very clearly andi got the answer of my question but i have one more querry. Let me explain. In your Pic you mention the L stack L0.0 and it is local variable and i far i understand it could be change in next scan cycle or could be effect due to previous block and change the L0.0 to some other Value Like Example L0.1. But in the program i use L0.0 to run the motor and due to Change its value from 0.0 to 0.1 the motor not running sometime. Pl. help me for the above solution. I make an FB of analogue value for scalling and displaying values in HMI. And this FB is calling in Different FC's. But sometime due to L stack memory address changes some of my Flipflop is not working. I hope you understand i Set/Reset flipflop through L stack memory address. And These addresses changes sometime. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/30/2019 2:04:45 PMNew subject after splitting |
|
Follow us on