(0)| 9/30/2008 8:53 AM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hi SMF1, when you use HW Siemens it will be shipped preconfigured and make you just have to do a lil work, but it possible use different HW too. Anywy better you use HW with same features, important are: - CPU - PCI slots nr. - graphic card model - original Microsoft Windows OS (not OEM or cumtom supplier release) - and RAM amount SO, you can use difeferent but noone can warranty you totally, better if you use station with same feature: New SIMATIC PCS 7 Industrial Workstations Type 547B with SIMATIC PCS 7 V6.1 + SP2 Released for Deliveryis equipped with Microprocessor: Intel Core 2 Duo E6600 / 2 x 2.4 GHz |
Follow us on