(0)| 2/25/2019 10:41 AM | |
|
Joined: 11/28/2017 Last visit: 9/9/2024 Posts: 3 Rating:
|
Hi all I'm in the process of learning STL but do have some issues. I'm trying to build a ladder NW (2) from a STL NW (14) but is in doubt about the significance of my result which deviates from the original STL. The result of my LADDER utilises JNB but NW 14 is set up with JCN. I believe that my NW2 does the same as NW14 but are not sure though. I've attached the screen dumps in a pdf file, "STL vs LAD 3"... BR laursen AttachmentSTL vs LAD 3.pdf (215 Downloads) |
| 2/25/2019 10:52 AM | |
|
Posts: 2826 Rating:
|
Hello. The LAD representation suits the purpose of your current use. The differences in the two JUMP instructions would have mattered if code was to follow the MOVE instruction. Have a look at the document: SIMATIC STEP 7 V5.5 Statement List (STL) for S7-300 and S7-400 Programming for detailed descriptions. BR |
| 2/25/2019 12:41 PM | |
|
Joined: 11/28/2017 Last visit: 9/9/2024 Posts: 3 Rating:
|
Okay - I see. does this apply only to the current FC or to the entire project? BR laursen |
Follow us on