(0)| 3/20/2019 8:54 PM | |
|
Posts: 1 Rating:
|
Hi All, I´m already have 2 HMI linked with the same S7300 and working pretty good but I´d like to use just one software application inside in both HMI but one of then (#1) need to enable/disable 3 buttons on second one (#2). The buttons are present in both HMI at the same tag. It mean probably I should send a command for just one MPI address... Could somebody help me how to do that? Regards ------------------------------------------------------------------------------------------ |
Last edited by: sergiosamy at: 3/20/2019 9:02:37 PMLast edited by: Jen_Moderator at: 3/21/2019 7:23:26 AMNew subject after splitting Last edited by: sergiosamy at: 3/21/2019 6:27:12 PM |
|
Follow us on