(0)| 3/29/2019 8:57 AM | |
|
Posts: 36 Rating:
|
Hi! I have the same problem, three DMM and one SMM, thats a total of 7 and to much. The system was with two DMM and one SMM in the first version. No problem. Now, i had to add to axes but the TIA v14 wont let me download the new configuration beacuse it is now 7 objects. The DMM module wich has only one motor is deactivated. How can I proceed? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/29/2019 11:34:33 AMNew subject after splitting |
|
| 3/29/2019 11:53 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Disable one motor is published within the conference SINAMICS. Best regards Jen_Moderator |
Follow us on