(0)| 9/10/2008 7:59 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hi Try to connect 35 simocode on the same profibus line. Read in manual SIMATIC NET PROFIBUS Networks said: "To increase the number of nodes (>32) in a network or to extend the cable length Also " ...When configuring an electrical network with RS-485 repeaters, the following About CP443-5ex. I hope this link will be helpfull: Description of the CP 443-5 Extended S7-CPs for PROFIBUS Configuring and Commissioning regards |
Follow us on