(0)| 4/4/2019 2:16 PM | |
|
Posts: 2 Rating:
|
HI, I have setup a yearly timer and assigned the On and Off times to VM Parameters. I have written a web page that shows the outputs from the Timer this allows me to write back to the timer from the web page. I cannot understand the VM values.: If I set the on Time as 1st Jan the VM value is 257 2nd Jan VM value shows 258 the 1st of Feb shows 513 The 31st Dec shows 4657 How do I work out the correct month and day from a single value. Please see attachment which should make it clear. Thanks AttachmentDoc1.pdf (283 Downloads) |
Follow us on