4/10/2019 2:13 AM | |
Posts: 8 Rating:
|
Hi, There is no screen created by LWE, the direct LOGO link between the PC and LOGO appears in the "LOGO BM" is the image of the simple LOGO (see attached file). I am using an Android emulator - Blue Stacks in order to simulate the screen of a Tablet in the PC, and this also does not appear the screens created when I use the connected Siemens APP WEB of the LOGO. In both situations I have the PC connected to the LOGO but there is no sign of the screens created (both the program and the screens have been transferred to the LOGO). Thank you for your help in this step of implementing the LOGO 8 functions. Thank you Ricardo Queiroz da Paz
AttachmentImagens - APP e no PC.pdf (311 Downloads) |
4/10/2019 7:21 PM | |
Joined: 12/18/2014 Last visit: 9/8/2025 Posts: 35934 Rating:
|
Do you set the check mark by "to customized site"? |
4/10/2019 7:26 PM | |
Joined: 12/18/2014 Last visit: 9/8/2025 Posts: 35934 Rating:
|
Please upload your LWE project. Then I'll make a test with LOGO! and my PC. |
4/10/2019 11:00 PM | |
Posts: 8 Rating:
|
Hi, Follow the LWE project with the 4 pages (I removed the photos of the equipment to make the file smaller), where are all the variables of the project. Thank you for your help Ricardo Queiroz da Paz AttachmentRack NAV Modelo 3.zip (258 Downloads) |
4/10/2019 11:15 PM | |
Posts: 8 Rating:
|
Hi, Please consider this LWE project file missing the setting in Navigation. Thank you Ricardo Queiroz da Paz
AttachmentRack Modelo 3.zip (231 Downloads) |
4/11/2019 6:48 AM | |
Joined: 12/18/2014 Last visit: 9/8/2025 Posts: 35934 Rating:
|
When I load your ORIGINAL LWE project to the LOGO!, I can only see page "Home Page". The other pages are not visible. That's because you did not link the pages to the navigator. I edited your project and linked the pages to the navigator. The edited project is attached as version V2. AttachmentRack NAV Modelo.zip (265 Downloads) |
Follow us on