3/14/2019 11:11 AM | |
Joined: 9/9/2015 Last visit: 4/9/2025 Posts: 732 Rating:
|
Dear Mahesh, I think you could override the SFC type/ the FB , to make sure the blocks in library is the same with the program folders first. Since you have imported one round, all FBs have been inserted in your project blocks folder. And if you created chart before, it should exist in chart folder as well. SFC type = FB, and the blocks in your chart is instance data block of the SFC type. You can try to copy the SFC type in your library (chart folder) and replace the SFC type in your project chart folder. If you wanna delete in proper way, delete all the related chart, and do a clean up in chart folder by going to CFC editor, option->block type -> clean up -> Highlight all, and remove. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
4/18/2019 5:57 AM | |
Joined: 10/3/2013 Last visit: 9/14/2024 Posts: 125 Rating:
|
I will check and revert you |
Follow us on