(0)| 4/16/2019 12:37 AM | |
|
Posts: 125 Rating:
|
I think the feature you're asking for isn't built into the firmware or runtime software. |
| 4/23/2019 3:34 PM | |
|
Joined: 10/11/2006 Last visit: 1/21/2026 Posts: 6052 Rating:
|
Hello, if you want to define Cartesian workspace zones for the path object, you can use the standard library "Handling Advanced". Within this library, a zone management is implemented and ready to use. SIOS Link: https://support.industry.siemens.com/cs/ww/en/view/85014317 if you just want to prevent that the single axes connected to the path object (path axes) are reaching a certain limit, you can use the software limit switch functionality of the TO Axis. You can parameterize it within the "Limits"-Mask of the TO Axis. Please Note: the software limit switches are only protecting the path axes from going into a certain limit. The tool center point (Cartesian position) is not protected. |
|
With best regards, |
|
Follow us on