(0)| 10/13/2008 9:01 AM | |
|
Joined: 4/24/2006 Last visit: 1/14/2026 Posts: 9105 Rating:
|
Dear Eric, Perhaps this link is useful: http://support.automation.siemens.com/WW/view/en/19865167 I think it is not possible using profibus. When using ethernet it is possibleto transfer datarecords to a PC. I'm not sure it will work between two MP377. Perhaps using OPC option? Best regards, Wizard |
| 10/13/2008 10:03 AM | |
|
Posts: 487 Rating:
|
Hi The link is interesting but not for my problem . It has to do with recipes and I have little knowledge of recipes.I presume that you attach x amount of tags to a recipe and send these 'updated 'tags to the PLC when you select a new recipe.What happens if you have two MP's ? Say you changed the recipe on the one and send the info to the PLC.Are the other MP's tags updated ? Or can you update/create new recipe via the PLC Another possible solution were are looking at is the install a ethernet cable between the two MP's or to manually export/import the recipes using a USB stick Greetings Eric |
| 10/13/2008 10:51 AM | |
|
Joined: 4/24/2006 Last visit: 1/14/2026 Posts: 9105 Rating:
|
Hi Eric, Perhaps this link will give you more information about recipes: http://support.automation.siemens.com/WW/view/en/23901413 You can export datarecords, from panel to PC (or USB stick). And import them on another panel (if the same recipe is used) Best regards, Wizard |
| 10/13/2008 12:40 PM | |
|
Posts: 487 Rating:
|
Hi I think for a interim solution we will go for the USB stick export/import. Eric |
Follow us on