(1)| 5/20/2019 11:18 AM | |
|
Posts: 2 Rating:
|
I am a student and i am very new to plc programming and i have a problem regarding temperature control using s7-200. my project is based on automating a thermal fatigue test stand. In detail, the machine have a heat source(for heating a metal), a hydraulic cylinder(to carry the metal up to the heater or down into the tank) and a water tank(for cooling the metal). I am required to control this process in which the cylinder should go up to the heater and stay up until the temperature is between the range of 95-99 degrees after which the cylinder should move down to the water tank and stay down until the temperature cools to the range of 39-44 degrees. i also have a thermocouple. i have read papers and watched videos, and below is attached of what i was able to do. please i need your help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/20/2019 13:44:36New subject after splitting |
|
| 5/24/2019 12:56 PM | |
|
Posts: 623 Rating:
|
Hi Cruizler, U will need to use PID block for heater control. Rest of the Logic is simple & needs only timers. |
This contribution was helpful to
|
|
| 5/24/2019 3:17 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Cruizler; Sample applications for the S7-200 PLCs have been grouped under the designatuion S7-200 Tips and Tricks; you can download them using the link in this thread: Here is Tip 46, Using TCs . Hope this helps, Daniel Chartier AttachmentTip #46 Using TCs.zip (592 Downloads) |
This contribution was helpful to
|
|
| 5/24/2019 3:18 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Cruizler; To follow up, here is TIP 54, PID LOOPs. Hope this helps, Daniel Chartier AttachmentTip #54 PID LOOPs.zip (578 Downloads) |
This contribution was helpful to
|
|
Follow us on