(0)| 5/24/2019 2:15 PM | |
|
Posts: 226 Rating:
|
Hello Scout v5.3.1, D425: Bootloader: D4xx_BOOT_V03.04 BIOS: V02.02.00.00 FPGA: 7.1.0 ----------------------------- D425 v4.1.5.6-->firmware update USB (Start device update tool) to v4.3.1.23 At the end of the update, I get an error and all the lights are flashing.error LED: RDY -red flashing LED (2 Hz) RUN, Stop, SU/PF, SF, DP1,2 =yellow flashing LED (0.5 Hz) OPT =LED off States of the 7‑segment display: 6 and Flashing point but when I copy the Kermel D ( archive (4.3.1.23) to the CF card, there are no problems with downloading ... AttachmentIMG_3619.MOV (324 Downloads) |
Last edited by: SAR-CNT at: 05/24/2019 14:30:54Last edited by: SAR-CNT at: 05/24/2019 14:46:01Last edited by: SAR-CNT at: 05/24/2019 14:48:26Last edited by: SAR-CNT at: 05/24/2019 14:50:28Last edited by: SAR-CNT at: 05/24/2019 14:56:46Last edited by: SAR-CNT at: 05/24/2019 15:15:44Last edited by: SAR-CNT at: 05/24/2019 15:18:50Last edited by: Jen_Moderator at: 05/27/2019 10:00:08Optimized link. |
|
| 5/25/2019 10:26 AM | |
|
Posts: 226 Rating:
|
Hello I found out the reason for the wrong FW archive which forms SCOUT V5.3.1 I have a concern in using Scout v5.3.1 |
Follow us on