6/11/2019 4:55 AM | |
Joined: 12/18/2014 Last visit: 9/18/2025 Posts: 36013 Rating:
|
Here is a small example of how you can calculate the total time of timers and compare it to the value of 48 hours (larger). The values of each timer are transferred to the VM memory via Parameter VM Mapping and then read in again via an analog network inputs. Please note: The time format of the timers is h: m. Therefore, the values in the timebase are minutes. 12 hours = 720 minutes, 48 hours = 2880 minutes. AttachmentCompare_sum_of_all_timers_0BA8.Standard.zip (319 Downloads) |
This contribution was helpful to
1 thankful Users |
6/11/2019 7:54 AM | |
Joined: 12/18/2014 Last visit: 9/18/2025 Posts: 36013 Rating:
|
It's not that bad that you have to apologize for that. |
This contribution was helpful to
1 thankful Users |
Follow us on