(0)| 6/26/2019 12:23 PM | |
|
Joined: 10/11/2006 Last visit: 1/21/2026 Posts: 6072 Rating:
|
Dear Manoj R The 12 pulse rectifier circuit exist of two 6 pulse rectifiers which voltages needs being shiftet for 30°. The simpliest way doing it is by making a three winding transformer, which secondary sides connected one in Y and the other in Delta. The delta cannot be grounded sensefuly, hence the Y windings arent grounded as well. So the total system is isolated and an isolation monitoring is requred! Please find Engineering Manual SINAMICS G130, G150, S120 Chassis, S120 Cabinet Modules, S150 |
|
With best regards, |
|
Follow us on