7/10/2019 5:10 PM | |
Joined: 5/14/2019 Last visit: 8/2/2023 Posts: 8 Rating:
|
I am trying to call the function on the top halve of the attached document multiple times in another function. This function works alone, but when I attempt to call it multiple times in the bottom only the first one works. I created two multi-instances of this function that are Query2 and Query5. Is there something I am doing wrong? Only the first Query2 ever seams to ever initiate the "Send_P2P" to receive the position. I also have a single instance of this function in my main routine that I use for manually receiving the position of the pump. Sorry about the sloppy code I am new at this and it is still a work in progress. AttachmentQuery_Function.txt (242 Downloads) |
Follow us on