(0)| 6/26/2019 2:19 PM | |
|
Posts: 3 Rating:
|
Hi all After set Nc MD20 to 2kb and format part program memory as mentioned in the manual. Then When we used BTR start softkey the alarm 3020 appare So How can I make sure if the option c69 is installed on the system or not?? 810m ga3 6fc3551-1ac-z CPU 6fx1138-5bb04 32kb menory If it was not installed .how I can activate or order it? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/26/2019 14:25:50New subject after splitting |
|
| 6/27/2019 8:05 AM | |
|
Joined: 10/17/2007 Last visit: 1/14/2026 Posts: 4574 Rating:
|
Alarm 3020 means your machine has No these option or setting lost You did not introduce the machine history.--is it running machine ? i #1--is it original has option C69 ( machine had Siemens controller log book, in which listed all options when machine builder purchased) #2--Or you want to add BTR function to the machine? C69 is NOT a free function ? If for #1 you need to contact Local Siemens , to get the option information recovered **810M/T is belong to 800 system.and most options in 800 system --are some MD bits setting if you have no option C69 , MD 20 is meaningless
|
Last edited by: nulizhang at: 06/27/2019 08:07:44If you like my comments please |
|
| 7/23/2019 10:39 AM | |
|
Posts: 1086 Rating:
|
Hi Maawadg6, please try the contact site, which you can find in the middle of the Page next to "Support Request": Contact Br, |
Last edited by: 8Noodles at: 07/23/2019 10:40:48 |
|
Follow us on