7/24/2019 2:50 PM | |
Joined: 7/3/2016 Last visit: 8/7/2025 Posts: 25 Rating:
|
Hi, the solution has two pc-device, one PH server with IS-Ready service running with the same user acount that the Information server who run in different pc-device. The connection with PH is realiable. I used the Report Builder (SQL tool) to edit an example of template file (.rdl) to get data with a filtering from a list of defined menssage numbers. It's work ok when tested agaisnt a OS-datebase. The Query of this template declare a structure of table with the only difference of timestamp format field when perform a consult to a PH server. But when a tried to do this, after 30 sec, I get the error of picture, if I do the query from Report Builder get more specific details that if I do from IS browser front-end. If I take a look to Activity Monitor of SQL Management Studio of database Instance of PH Server I see the query came in from the IS in the section "Recent Expensive Queries". The full-text of error is this: [snip] Any suggest will be gratefull!! Attachmentfiles.zip (85 Downloads) |
Last edited by: alanisgp at: 07/24/2019 14:51:34Last edited by: Jen_Moderator at: 07/25/2019 05:45:50Added error message as an txt file. Added all files as a zip-file. |
|
Follow us on