(0)| 7/24/2019 9:15 AM | |
|
Posts: 39 Rating:
|
Hello to you all, Systems used: - Win 10 Pro, Simotion Scout V5.2.1.0 (SA). I would like to ask if someone could help me on this topic of U7ITRCAX.ocx issue. The problem is that when I try to trace a variable in time diagram before entering the device trace an Error shows for U7ITRCAX (picture attached [capture_001]). This error shows 3xtimes so I guess that it got problems when starting Time diagram, FFT diagram and bode diagram (all three are affected, please refer to picture [capture_002]). Measuring is able to start but I cannot monitor or to import any diagram curves to the project. Created even multiple times new projects, but it didn´t help. Is there an additional driver missing or is there a way to work around the problem? Thank you very much for the info. With regards, Tech-Core AttachmentArchive.zip (444 Downloads) |
Last edited by: Tech-Core at: 07/24/2019 09:17:34 |
|
Follow us on