(0)| 8/5/2019 3:38 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello Simatic Manager is used to program S7 PLCs, not S5.CPUs, and the addresses you show are also for a S7-300 or S7-400 PLC. You might be posting in the wrong conference. In any case, neither the S5 or the S7 PLCs have a mapping instruction such as you are looking for. By order of decreasing ladder betworks: - You can use LAD instructions to set output bits one by one based on the value of individual input registers. - You can also transfer complete bytes, words or Dwords from the input area to the output area using the Move instruction. - Or you can use SFC 20 BLKMOV to transfer large amount of data between the input area to the output area. You will find SFC 20 in the SFC/SFB instruction library of Step 7(v5.x) , and use the On;ine hel;p or the following manual to get detailed information on its use: SIMATIC System Software for S7-300/400 System and Standard Functions - Volume 1/2 Hope this helps, |
Follow us on