(0)| 8/7/2019 2:16 PM | |
|
Joined: 8/3/2009 Last visit: 1/21/2026 Posts: 16653 Rating:
|
Hello With which PLCs do you use the Comfort Panels? If you use for example S71500 PLCs then I would use the NTP Sxnchonisation from the Time Master to the S71500 PLc s and the PLCs are Masters for the Panels. This is the best way, because the Comfort Panels cannot perform a autmoatically Summer/Wintertime Change by their own. the need always a PLC to do it: -< LINK Like This: PC with NTP MAster ->(NTP) -> PLC->(S7Channel as Slave) -> HMI Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on