(0)| 8/6/2019 6:21 PM | |
|
Posts: 6 Rating:
|
Hi, Can I communicate panel with two PLC (schneider, siemens) Schneider use modbus tcp/ip Siemens S7300/400 ethernet |
| 8/6/2019 7:33 PM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello bilelplc; Most Siemens operator panels also have a Modbus TCP channel, as masters (clients). Can your Schneider model work as a slave (server)? Or do you know of a commercial coupler between 2 Modbus TCP clients? Could you use OPC drivers between the 2 panels? The screenshot below is taken from the Simatic Comfort operator panels system manual, as an example. https://support.industry.siemens.com/cs/ww/en/view/49313233 But what exactly are you hoping to exchange between the 2 panels? Information on the exact model of panels and programming software you are planning to use (both for the Siemens and the Schneider panels) would allow us to limit the scope of our replies. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 08/06/2019 19:41:00 |
|
This contribution was helpful to
|
|
Follow us on