8/8/2019 11:02 PM | |
Posts: 2 Rating:
|
Hi! My first project, so be gentle 1. Kompressor I will start the kompressor with a switch, that start a timer and makes it run for 2min. It will have a pre warning, that starts a red lamp after 1:30min has passed. But if i press the switch before the time is up it doesn't restart the pre warning timer, only the 2min time for the kompressor. How do i fix this? 2. Lightning in garage I will have a impuls switch that has to be pushed, before the timer for lightning is turned on, ie. the motion detector can't start the light before the switch is turned on. But the motion detector should also restart the timer when it got a motion detection. How to fix this? 3. Exterior lightning Main lightning is started and stopped with the astronomical clock. Secondary lightning is started with a motion detector, that starts a 5min timer . With the astro clock condition. AttachmentGaraget2.zip (281 Downloads) |
8/9/2019 9:39 AM | |
Posts: 2 Rating:
|
Hi there ixo! I'll try and explain.. The lightning switch should turn on(with timer) and off the light, and make the motion detector work(also with timer) |
8/9/2019 9:56 AM | |
Joined: 12/18/2014 Last visit: 9/17/2025 Posts: 35968 Rating:
|
I'm sorry, I do not understand that. Since I can only guess what you want. AttachmentGaraget2_V2.zip (285 Downloads) |
Follow us on