(0)| 8/26/2019 4:19 PM | |
|
Posts: 4 Rating:
|
I'm investigating the Opener library however without success, it seems to be the library is a emulator for ETHERNET/IP thar create a PLC node , testing with Node-red by module eth-ip onto IOT2000, however, I can not conect directly them to get for any tags , show the following message : "[eth-ip endpoint:342e217.4d937de] Error connecting to PLC: Error: timeout occurred while reading Controller Props. I hope after this will be to be possible to send for MQTT broker. Any way, if anyone get in over tags from IOT2000 using node red, based on node eth-ip ? Best Regards. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/27/2019 08:15:24New subject after splitting |
|
Follow us on