(1)| 9/4/2019 8:17 PM | |
|
Posts: 20 Rating:
|
Hi! I have an automation project that consists of projecting a controller for aircraft maintenance platforms. Until now, I thought the best option was having a PLC (S7-1200 CPU 1215C) for each platform. For example, considering I have two fuselage platforms (identical, one for each side), then I would have two PLCs. For each platform, I also have multiple sensors that I'm planning on connecting to IoT2040 (again, one IoT per platform). Each IoT connects via Ethernet with the respective PLC. Is it possible to use only one PLC for both platforms? Is it possible to establish a wireless connection between the two IoTs and the PLC? Thank you in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/05/2019 06:49:26New subject after splitting |
|
Follow us on