(2)| 9/10/2019 7:32 AM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hi ANTONIO7765, You basically have two options: Download change and Download full In case of small changes in CFC (adding blocks, change logic etc.) you can compile the CFC charts and download change to the CPU. In case of expanding blocks like adding I/O to an existing block type, you may need to download the CPU in stop. In that case you must execute a full download where the whole program is downloaded again to the CPU. With the CPU410, you have the option to execute TCiR. This means you can download type changes in run. In PCS7 V9.0 there is only one scenario where you cannot use TCiR: Changing the MsgEvID attribute. But in all other cases, you can download in Run. So downloading change is your quickest solution. |
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on