(0)| 10/24/2008 5:06 PM | |
|
Posts: 1 Rating:
|
How can I setup 2 S7 300 Cpu or CPU314C-2Dp via MPI connection and get the data from another cpu? |
| 10/27/2008 9:33 PM | |
|
Posts: 487 Rating:
|
There are different possibilities. simplest being global data communication. There are some are some communicaton blocks with s7 basic communication. Check the link below. http://support.automation.siemens.com/WW/view/en/20982954 It has also link to other helpful links. Which function is used depends on the application, criticallity and the required amount of data. |
| 10/29/2008 11:42 PM | |
|
Posts: 5822 Rating:
|
Hello Jemirah, would you mind checking this FAQ, I think it will answer your questions quite well: Options for communications via MPI Best regards J_Bell |
Follow us on