10/7/2019 11:13 AM | |
Posts: 45 Rating:
|
But how will it work out? Every change of state will trigger the sequence? Or it will be done automatically? |
10/8/2019 5:02 PM | |
Joined: 5/2/2016 Last visit: 7/7/2025 Posts: 19 Rating:
|
Hi, this depends on which s7 input node you use. I would recommend using the input node from "node-red-contrib-s7". There you can decide whether you want to trigger the flow cyclically so for example every 100ms or only when the value of the variable changes. Then you also need a function node between the s7-input node and the http-request node which only emits a value (triggers the http-request node) if the digital input is pressed or rather the variable is true. |
Follow us on