(0)| 10/24/2019 2:11 PM | |
|
Posts: 6 Rating:
|
hi i have the same problem. created in SP3 and migrated automatically to SP5, the project is with non error and i can download to the runtime system in the pc but still no connection with simotion D435 fw 4.5. I had to upgrade the runtme on the pc from SP3 to SP5 too, and at least install the update 1 (hotfix) but still doesn't work. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/25/2019 08:26:46New subject after splitting |
|
| 10/24/2019 3:27 PM | |
|
Joined: 5/12/2006 Last visit: 1/16/2026 Posts: 22827 Rating:
|
hello, check settings for PG/PC Interface in windows control panel on the winccflex rt system. regards christoph |
Follow us on