11/8/2019 11:21 AM | |
Joined: 1/3/2019 Last visit: 7/10/2025 Posts: 1 Rating:
|
HI, I'm having trouble installing opcua package on IoT 2040. I got this messege shown: npm ERR! Linux 4.4.154-cip28 npm ERR! argv "/usr/bin/node" "/usr/bin/npm" "install" "-g" "node-red-contrib-opcua" npm ERR! node v6.14.3 npm ERR! npm v3.10.10 npm ERR! code ELIFECYCLE npm ERR! node-opcua-client@0.7.4 postinstall: `node test_helpers/create_certificates.js certificate -s -o certificates/client_selfsigned_cert_2048.pem` npm ERR! Exit status 1 npm ERR! npm ERR! Failed at the node-opcua-client@0.7.4 postinstall script 'node test_helpers/create_certificates.js certificate -s -o certificates/client_selfsigned_cert_2048.pem'. npm ERR! Make sure you have the latest version of node.js and npm installed. npm ERR! If you do, this is most likely a problem with the node-opcua-client package, Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/08/2019 12:25:19New subject after splitting |
|
11/8/2019 12:37 PM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, Please refer to the installed version of opcua-nodes in this thread as these are compatible with NodeJS v6. Kind regards! |
Follow us on