11/13/2019 7:52 AM | |
Posts: 2 Rating:
|
dear all , Greetings please your help ,I have three distributed water tanks the distance between every one and the supply pumps around 3 km so i try to make wireless communication between three slave logo_8 and the master one which near to pumps which will revive the water level signals from the three tanks ,I already made the program and the network between the four logos but during make drag drop for network input NI and network output NQ the sequential serial of NI jump direct from NI11 to NI13,NI12 not inserted and when i have try to make download to logo message came there blocks without connection to output although i removed the program and wrote again Attachmentlogo_8.pdf (275 Downloads) |
11/13/2019 8:02 AM | |
Joined: 12/18/2014 Last visit: 9/22/2025 Posts: 36024 Rating:
|
Hello hesham99, at first welcome to the forum. Please be so kind and don't post twice or more for the same problem. You also post here (4th reply): Please can you upload your programs. The we can take a look. A screenshot of the message alone is not helpful. |
Last edited by: ixo65 at: 11/13/2019 08:02:41 |
|
Follow us on