(0)| 11/14/2019 5:55 PM | |
|
Posts: 137 Rating:
|
Hi all, I am using a Position axis technology bock with TIAv15.1 and CPU 1510 3pn and S110 drive. I have selected encode as "mounted on motor side" and the software limit in the technology block as "-100 mm to +100 mm" The motor with go over 100 (approx 100.20) and then stop which will give an error of software limit reached . Error code 534 (this error only comes when you go over SW limits) When I change the encode mounting to "mounted on load side it works fine , it stops exactly at 100 mm and does not go over it.(but there are other issue associated with mounting at load side and I cannot use mounting at load side) any idea why the measurement goes over software limit when I use encoder mounting at motor side, Please feel free to ask any clarification. PS - "I am very new to technology block" I have attached image of all the setting done in configuration window of technology block AttachmentImages.zip (170 Downloads) |
Last edited by: Divej93 at: 11/14/2019 18:00:44 |
|
Follow us on