(2)| 11/20/2019 6:07 AM | |
|
Joined: 9/9/2015 Last visit: 12/5/2025 Posts: 732 Rating:
|
Dear ashadako, You can define the I/O as a parameter in Process object view by 1. Open Process Object View 2. Click on the folder or chart you want 3. click on the Parameter View in the right hand pane of the POV 4. right click on the number column , you should see Process Object / select I/Os. 5. Filter: Select I/Os dialog box will pop out, you may set some filter rules or select All 6. All the Input and Output , with or without parameter in the chart/folder that you have selected in step 2 will be shown in this view. 7. look for the Input/output you want, set it to Parameter (interconnection,settings), or Signals (link to hardware address/ DB address). 8. Then press Ok and F5 to refresh. Done. Hope it is helpful for you. |
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
|
|
Follow us on