(1)| 11/19/2019 4:29 PM | |
|
Posts: 20 Rating:
|
Thanks a lot, I'll try it. |
| 11/20/2019 8:29 AM | |
|
Posts: 181 Rating:
|
Hello, I just want to give some explanations about the motor replacement. If the new motor has the same article number as the motor to be replaced, then the SINAMICS S210 will not show any fault or warning. Currently, there is no parameter that can activate monitoring for the motor serial number or the motor serial number can not be read out via parameters. Additional hint: A motor with a singleturn encoder AS22DQC (1FK2☐☐☐_☐☐☐☐☐-☐S☐☐) can be replaced by an otherwise identical motor with a multiturn encoder AM22DQC (1FK2☐☐☐_☐☐☐☐☐-☐M☐☐) without having to recommission the drive system. Further information about the motor replacement can also be found in the operation instructions SINAMICS S210 / SIMOTICS 1FK2, Chapter “10.1.2 Replacing the motor”: https://support.industry.siemens.com/cs/ww/en/view/109771824 Best Regards, Technical Support for SINAMICS S210 |
This contribution was helpful to
|
|
Follow us on