(0)| 11/18/2019 4:29 PM | |
|
Joined: 10/19/2016 Last visit: 7/11/2025 Posts: 316 Rating:
|
Hi sirs, i have a test station with a 840Dsl connected to a 1PH7 motor. i'm connecting to it different products with same characteristics. In particular the spindle axis has only the second measurement system active with an encoder like this. It has always worked but today i receive the error attached. the connections and the shields are OK. If i rotate by hand the spindle i can see the speed on the display. What can i do? |
|
𓋹 Siemens 840Dsl + TIA v17 𓋹 |
|
Follow us on