(0)| 11/26/2019 9:03 AM | |
|
Joined: 11/23/2007 Last visit: 11/4/2025 Posts: 133 Rating:
|
Have you a faq or how to description to do this with starter. |
| 11/26/2019 11:43 AM | |
|
Posts: 181 Rating:
|
Hi Nico, Could you please tell me what combination of PLC and drive (S210) and also Telegram you are using? Have you tried to run a test without OBT (One Button Tuning)? On the other hand, could you try to make a One Button Tuning based on factory reset and set before enabling the OBT the parameter p5271 (One Button Tuning configuration) bit 04 (Setting the torque precontrol) to “NO”? We offer an optimization guide for drives, which also contains the SINAMICS S210 with it´s possible settings on One Button Tuning dynamics (see Chapter 15.2 S210): https://support.industry.siemens.com/cs/ww/en/view/60593549 additional Note: The SINAMICS S210 drive system is fully integrated in TIA STARTDRIVE V15.1 or later, but a support of SINAMICS STARTER (classic) is not provided. See also FAQ: https://support.industry.siemens.com/cs/ww/en/view/109761460 Best Regards, |
Last edited by: TechSupport SINAMICS S210 at: 11/26/2019 11:44:43 |
|
Follow us on