(2)| 12/10/2019 6:59 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, The first message: Waiting for Batch data is normal. This is because you have installed Simatic BATCH, but did not load a batch project to the server yet. The second, i'm not sure why you cannot select PCS7 OS. Did you get any errors while installing PCS7? Did you install a package option? Like Single Station System or Engineering package? Or did you install all software separately during the install of PCS7? Can you try to open a sample project via File->Open->Tab: Sample Projects->Select APL_Example_EU and then try opening the OS project? |
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on