(0)| 1/9/2020 10:44 AM | |
|
Joined: 9/30/2016 Last visit: 1/12/2026 Posts: 953 Rating:
|
Please also see the attached screenshots. I need to verify that a meter-counter with an encoder is calculating the meters with the correct formula. Number of pulses per revolution of the wheel (#Encoder01Pulser) Number of meters per revolution of the wheel (#Encoder1.Meter) Number of pulses received (#Encoder1.Conut) How many revolutions has the wheel done (#Encoder1.Turns) How big a fraction of a revolution have the wheel done (#Encoder1.Fine) The calculation should be simple (#Encoder1.Turns + #Encoder1.Fine) * #Encoder1.Meter I can see where #Encoder1.Turns and #Encoder1.Fine are calculated but not where that are added or multiplied. Can one of the boardmembers help me see it or convert it to Function Block or Ladder logic? AttachmentFB1 Enc.zip (269 Downloads) |
| 1/9/2020 2:49 PM | |
|
Joined: 9/30/2016 Last visit: 1/12/2026 Posts: 953 Rating:
|
Hello Kashir, Thank you for answering. Please see the attcahed screenshots of the interface for both FB's.
AttachmentFB1 Enc1.zip (254 Downloads) |
Follow us on