(0)| 1/17/2020 2:13 PM | |
|
Joined: 2/1/2010 Last visit: 1/14/2026 Posts: 218 Rating:
|
I hope you mean PCS7 8.2 with CFC 8.2 SP1. As you typed it PCS7 8.0, is not compatible with CFC 8.2 SP1. Assuming above is not the problem: Is it new PC or upgraded PC for the ES? If you haven't migrated the blocks to PCS7 8.2 library then you must install the 8.0 library back after installing PCS7 8.2. Or you can migrate the blocks according to the upgrade with new functionality procedure. |
|
If my post helped you, please rate. Thanks. |
|
| 1/20/2020 8:20 AM | |
|
Joined: 6/23/2008 Last visit: 1/16/2026 Posts: 1174 Rating:
|
Hello banconi,
from your answer I'm still not sure if you have PCS7 V8.0 SP2 and CFC 8.2 SP1 installed now or PCS7 V8.2 and CFC 8.2 SP1. If your actual installation is PCS7 V8.0 SP2 and CFC 8.2 I fear that this was not a good idea, as this combo is really incompatible. You can check it here with the Compatibility Tool. So, hopefully you created a backup from the ES and from the project before you did the update... Best regards... |
|
"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
Follow us on