(2)| 2/1/2020 11:47 PM | |
|
Posts: 30 Rating:
|
Hello mesnowball, Please find attached the link , detailed documentation of the APL block . APL documentation https://cache.industry.siemens.com/dl/files/967/109754967/att_939377/v1/s7jal90b_en-US.pdf |
| 2/2/2020 8:13 AM | |
|
Posts: 35 Rating:
|
Hi Tejaswi, thanks for the link to document.. I have some questions from the document. 1) Is it that i must set the “safepos” to 0 = open 2) what does it means 2= stop? Is it if I set “safepos” = 2, when protection or interlocks activated, the valve will stop at the position where it is? example if it is closed will remain as closed. If open will remain as open. If mid travel will stop at mid travel? Many thanks with regards, snowball
|
Follow us on