(4)| 2/4/2020 8:13 AM | |
|
Posts: 17 Rating:
|
Hi All, I have a file which is .ap15. I tired to open it with WinCC but unable to do so. I've received an error message which is "The file MDR_Stinger_30_08 V15.ap15 is not a recognizable format." Can anyone advise me on methods to open the file? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/04/2020 10:40:58New subject after splitting |
|
This contribution was helpful to
|
|
| 2/4/2020 10:43 AM | |
|
Joined: 12/18/2014 Last visit: 1/21/2026 Posts: 36503 Rating:
|
You can't open a TIA V15 file with WinCC flexible. |
| 2/4/2020 10:47 AM | |
|
Posts: 17 Rating:
|
Noted, I'll just have to wait for the upgrade then. Thank you very much. |
| 2/4/2020 10:51 AM | |
|
Joined: 5/12/2006 Last visit: 1/21/2026 Posts: 22829 Rating:
|
which update you mean? |
| 2/4/2020 12:00 PM | |
|
Posts: 17 Rating:
|
I see. I guess for now I wont be able to test it out until I upgrade it. Thank you for your support. |
| 2/4/2020 12:15 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello Walter; This thread is confusing. The answers you have gotten in this thread point to the fact that you need WinCC (TIA Portal) v.15 to open the HMI program contained in the .ap15 file. Are you trying to do so with WinCC Flexible? What software and which version are you using actually? You have already been told that there are no upgrades from WinCC Flexible to WinCC v.15. WinCC v15 must be purchased and licensed individually. What exactly were you expecting as an upgrade? What is available is a trial download of WinCC v15, with a temporary license valid for 14 days. Once installed, it would allow you to open and manipulate the .ap15 file you have. But eventually the trial license must be upgraded to a permanent license of the level you need (WinCC Basic, Comfort, Advanced or Professional). https://support.industry.siemens.com/cs/bg/en/view/109752566 Hope this helps, |
This contribution was helpful to
|
|
| 2/5/2020 1:16 AM | |
|
Posts: 17 Rating:
|
My apology, I meant upgrade by purchasing license for Simatic WinCC v15 along with TIA Portal V15. Or do I just need the WinCC V15 without the TIA Portal V15? Currently I'm using Simatic WinCC flexible 2008 SP3 (build: V1.4.0.0_1.16.0.16. |
| 2/5/2020 3:27 AM | |
|
Joined: 7/5/2013 Last visit: 1/21/2026 Posts: 3277 Rating:
|
Hello Walter, there is no WinCC V15 without TIA portal. TIA portal can contain WinCC and/or Step 7. For getting TIA V15 see the following link: SIMATIC STEP 7 and WinCC V15 TRIAL Download Regards, Frink |
|
Pi is exactly three! |
|
Follow us on